FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25 Rugged > Using the rugged model in rain
FAQ
Using the rugged model in rain
Can the rugged model be used in rain?
Answer
The front face of the rugged model conforms to IP66F and IP67F.
Therefore, the rugged model can be used in rain when the following conditions are satisfied.
・ perating ambient temperature -20°C to 65°C
・ Operating ambient humidity 10% RH to 90% RH, non-condensing
When raindrops hit the control panel hard, the touch switch may malfunction. Do not expose the operation panel to raindrops.
Avoid using the GOT in the environment of high humidity all the time.
Therefore, the rugged model can be used in rain when the following conditions are satisfied.
・ perating ambient temperature -20°C to 65°C
・ Operating ambient humidity 10% RH to 90% RH, non-condensing
When raindrops hit the control panel hard, the touch switch may malfunction. Do not expose the operation panel to raindrops.
Avoid using the GOT in the environment of high humidity all the time.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model
- Series
- GOT2000 Series