FAQ


FAQAbout Products
- FAQ > Drive Products > AC Servos-MELSERVO > MELSERVO-J4 > Wrong connection of servo amplifier power supply
FAQ
Wrong connection of servo amplifier power supply
I connected the main circuit power supply (L1, L2, L3) to the servo motor power input (U, V, W) oppositely and turned the power on. Can I continue to use the system if I fix the wiring?
- Category :
Answer
The system is probably malfunctioning and is in dangerous condition. Do not use it.
For repair, contact your local sales office.
- Product Name
- AC Servos-MELSERVO
- Series
- MELSERVO-J4, MELSERVO-JE, MELSERVO-J3, MELSERVO-JN, MELSERVO Others