FAQ


FAQAbout Products
- FAQ > Drive Products > AC Servos-MELSERVO > MELSERVO-J4 > Relationship between rotary switch and axis number
FAQ
Relationship between rotary switch and axis number
What is the relationship between rotary switch of MR-J4-B and axis control number?
- Category :
Answer
When the rotary switch is “0”, the 1st axis and is “1”, the 2nd axis. When the rotary switch is “A”, the 11th axis and is “F”, the 16th axis.
In combination with the auxiliary axis number setting switch, up to 64 axes (MR-J3: 16 axes) can be set.
In combination with the auxiliary axis number setting switch, up to 64 axes (MR-J3: 16 axes) can be set.
- Product Name
- AC Servos-MELSERVO
- Series
- MELSERVO-J4