FAQ


FAQAbout Products
- FAQ > Medium-voltage Power Distribution Products > Protection Relays > Protection Relays - MELPRO-A Series > Combination transformer
FAQ
Combination transformer
Is there a distance limitation between MPD-3 type ZVT and a relay?
Answer
It is required that the resistance is lower than 5 ohm for a go and return length using sealed cables. Other than MPD-3 type ZVT, it is similar to the distance between MZT type ZCT and a relay.
- Product Name
- Protection Relay
- Series
- MELPRO-A Series