FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > External appearance of the F2-40BL
FAQ
External appearance of the F2-40BL
The shapes of the F2-40BL battery differ between the one installed and the one separately available (spare part).
- Category :
Answer
Some of the F2-40BL batteries installed to a programmable controller are mounted on the printed circuit board. The separately available F2-40BL batteries (spare parts) are not mounted on a printed circuit board. The both types have the same function.
- Product Name
- F2-40BL
- Product Category
- Accessories, Options
- Series
- FX2N