FAQ


FAQAbout Products

- FAQ > Low-voltage Power Distribution Products > Low-voltage Circuit Breakers > Molded Case Circuit Breakers > degrees of protection to IEC60529
FAQ
degrees of protection to IEC60529
What is degrees of protection for MCCB, ELCB, ACB according to IEC60529?
Answer
The degess of protection for ACB is IP20 as standard (under the condition that front door is closed). For MCCB and ELCB, the degrees of protection can be IP20 with terminal cover as seen from front-side. Refer to the figure as below.
- Product Name
- Molded Case Circuit Breakers
- Series
- WS-V