FAQ


FAQAbout Products
 - FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > Number of FX3U-ENET-ADP Ethernet communication special adapters that can be connected to the FX3U series
 
FAQ
Number of FX3U-ENET-ADP Ethernet communication special adapters that can be connected to the FX3U series
How many FX3U-ENET-ADPs can be connected to the FX3U series?
    - Category :
 
Answer
One FX3U-ENET-ADP can be connected at the last stage (left end) of adapters for the FX3U series.
*The FX3U-ENET-ADP is a communication special adapter and occupies one communication channel. Therefore, when the FX3U-ENET-ADP is connected to the FX3U series, another expansion board/special adapter (including the FX3U-8AV-BD/FX3U-CF-ADP) can be used.
  *The FX3U-ENET-ADP is a communication special adapter and occupies one communication channel. Therefore, when the FX3U-ENET-ADP is connected to the FX3U series, another expansion board/special adapter (including the FX3U-8AV-BD/FX3U-CF-ADP) can be used.
- Product Name
 - MELSEC-F Series
 
- Product Category
 - FX3U
 
- Series
 - Main Unit