FAQ


FAQAbout Products
- FAQ > Industrial Computer > Industrial Computer MELIPC > MI2012-W(-CL) > Regarding failure of maximum resolution setting of MELIPC
FAQ
Regarding failure of maximum resolution setting of MELIPC
I have connected a display that supports MELIPC's maximum resolution, but I cannot select the maximum resolution
in the "Display resolution" setting of Windows. What could be the cause?
in the "Display resolution" setting of Windows. What could be the cause?
Answer
If you connect a display using a converter such as a display switch or DisplayPort-HDMI converter adapter,
you may not be able to select a high resolution. Refer the following points.
・ Connect the display directly to the MELIPC
・ Replace the converter
you may not be able to select a high resolution. Refer the following points.
・ Connect the display directly to the MELIPC
・ Replace the converter
- Product Name
- MELIPC
- Series
- MI5000
MI2000
MI1000