FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the connection between FX5-CCLGN-MS and SLMP-compatible devices
FAQ
Regarding the connection between FX5-CCLGN-MS and SLMP-compatible devices
What is the frame format when communicating between FX5-CCLGN-MS and SLMP-compatible devices? And what should I set?
Answer
The SLMP communication frames supported by the FX5-CCLGN-MS are 3E and 4E frames.
When SLMP communication is performed from an SLMP-compatible device to the FX5-CCLGN-MS, communication can be performed by setting the destination port to the SLMP communication port number of the FX5-CCLGN-MS in the settings of the SLMP-compatible device.
(Transmission requests from FX5-CCLGN-MS to SLMP devices are not allowed.)
For the port number to be set, please refer to the following manual.
MELSEC iQ-F FX5 User's Manual (CC-Link IE TSN)
When SLMP communication is performed from an SLMP-compatible device to the FX5-CCLGN-MS, communication can be performed by setting the destination port to the SLMP communication port number of the FX5-CCLGN-MS in the settings of the SLMP-compatible device.
(Transmission requests from FX5-CCLGN-MS to SLMP devices are not allowed.)
For the port number to be set, please refer to the following manual.
MELSEC iQ-F FX5 User's Manual (CC-Link IE TSN)
- Product Name
- FX5-CCLGN-MS
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series