FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the connection between FX5-CCLGN-MS and inverter
FAQ
Regarding the connection between FX5-CCLGN-MS and inverter
Communication is not established even if an inverter supporting CC-Link IE TSN is connected to FX5-CCLGN-MS. Is there a solution?
Answer
FX5-CCLGN-MS supports 1 Gbps communication speed with firmware version: 1.010, and 1 Gbps and 100 Mbps communication speed for version 1.010.
If the communication speed of FX5-CCLGN-MS is set to 1 Gbps, communication will not be established if an inverter with a communication speed of 100 Mbps is directly connected. Use a CC-Link IE TSN Class A-compatible switching HUB to convert the communication speed.
*Check the CC-Link Association website for recommended switching HUBs.
If the communication speed of FX5-CCLGN-MS is set to 1 Gbps, communication will not be established if an inverter with a communication speed of 100 Mbps is directly connected. Use a CC-Link IE TSN Class A-compatible switching HUB to convert the communication speed.
*Check the CC-Link Association website for recommended switching HUBs.
- Product Name
- FX5-CCLGN-MS
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series