FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the number of expansion adapters and expansion board connections for FX5S CPU module
FAQ
Regarding the number of expansion adapters and expansion board connections for FX5S CPU module
Up to how many expansion adapters and boards can be connected to the FX5S CPU module?
Answer
Up to 6 devices can be connected.
Extension adapters/boards (Max. 2 units) + analog extension adapters (Max. 4 units).
Extension adapters/boards (Max. 2 units) + analog extension adapters (Max. 4 units).
*Using an SD memory card module does not reduce the number of connections mentioned above.
- Product Name
- FX5S
- Product Category
- CPU Module
- Series
- MELSEC iQ-F Series