FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the communication execution status output device for ADPRW instructions
FAQ
Regarding the communication execution status output device for ADPRW instructions
Are (d2)+1 (ON upon normal completion of instruction) and (d2)+2 (ON upon abnormal completion of instruction) of the communication execution status output device of the ADPRW instruction automatically turned OFF?
Answer
It does not turn OFF automatically. Use the RST command in the program to turn it OFF.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series