FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the differences between CC-Link IE TSN and CC-Link IE Field Networks
FAQ
Regarding the differences between CC-Link IE TSN and CC-Link IE Field Networks
What is the difference between a CC-Link IE TSN and a CC-Link IE field network?
Answer
(1)Whether or not networks can be mixed on the same trunk line is different.
CC-Link IE TSN allows network mixing on the same trunk line. When using a CC-Link IE field network and TCP/IP communication, you must wire each network separately.
(2)The communication method is different.
The CC-Link IE TSN is a time-synchronized method, and the CC-Link IE field network is a token-passing method.
CC-Link IE TSN allows network mixing on the same trunk line. When using a CC-Link IE field network and TCP/IP communication, you must wire each network separately.
(2)The communication method is different.
The CC-Link IE TSN is a time-synchronized method, and the CC-Link IE field network is a token-passing method.
- Product Name
- FX5-CCLGN-MS, FX5-CCLIEF
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series