FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding Instruction processing time when the program capacity: 128 K steps are set
FAQ
Regarding Instruction processing time when the program capacity: 128 K steps are set
What is the instruction processing time when the FX5U/FX5UC CPU module is set to program capacity: 128 K steps?
Answer
LD instruction: 0.35 μs, MOV instruction: 0.779 μs. For other instructions, see the manual below.
MELSEC iQ-F FX5 Programming Manual (Instructions, Standard Functions/Function Blocks)
- Product Name
- FX5U, FX5UC
- Product Category
- CPU Module
- Series
- MELSEC iQ-F Series