FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding using the 2nsec Clock Timer
FAQ
Regarding using the 2nsec Clock Timer
How do I use the SM414(2n second clock)?
Answer
The value of n can be set in SD414, and the range is from K1 to K32767. (Default value: K30)
If n=K1, it is a 2-second clock timer with 1 second ON/1 second OFF.
If n=K1, it is a 2-second clock timer with 1 second ON/1 second OFF.
- Product Name
- FX5U,FX5UC,FX5UJ,FX5S
- Product Category
- CPU Module
- Series
- MELSEC iQ-F Series