FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding Statement and Note Types
FAQ
Regarding Statement and Note Types
What is the difference between 'PLC' and 'Peripheral' in the type of statements and notes?
Answer
PLC :it is written to the CPU module and consumes the number of steps.
・Without character - 3 steps
・With character : 4 + (Number of characters + 2 + 14) / 15 + Number of characters (steps)
・Without character - 3 steps
・With character : 4 + (Number of characters + 2 + 14) / 15 + Number of characters (steps)
Peripheral : Not written in the CPU module and is saved as additional program information.
・One line consumes one step.
・An asterisk (*) is automatically placed in front of the entered text.
・One line consumes one step.
・An asterisk (*) is automatically placed in front of the entered text.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Engineering Software
- Series
- MELSEC iQ-F Series