FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding MODBUS Device Allocation Settings
FAQ
Regarding MODBUS Device Allocation Settings
I use the MODBUS communication master function, but do I need to set MODBUS device allocation?
Answer
No need.
The MODBUS device allocation settings are used when the MODBUS slave function is used.
The MODBUS device allocation settings are used when the MODBUS slave function is used.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module,Network/Communication
- Series
- MELSEC iQ-F Series