FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding setting up encrypted communication (TLS) for FX5-ENET
FAQ
Regarding setting up encrypted communication (TLS) for FX5-ENET
Where do I configure the encrypted communication (TLS) settings for the MQTT communication and email functions of FX5-ENET?
Answer
In GX Works3, set the FX5-ENET module parameters from Basic Settings - External Device Configuration Settings.
In the "Ethernet Configuration" screen, select "Mail server connection module" or "MQTT connection module" from "Module list" - "Ethernet device (General)."
After selecting, you can enable encrypted communication (TLS) by setting the protocol to "TLS."
In the "Ethernet Configuration" screen, select "Mail server connection module" or "MQTT connection module" from "Module list" - "Ethernet device (General)."
After selecting, you can enable encrypted communication (TLS) by setting the protocol to "TLS."
- Product Name
- FX5-ENET
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series