FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding QoS, Retain, Will, and Clean Session Functions for MQTT Communications
FAQ
Regarding QoS, Retain, Will, and Clean Session Functions for MQTT Communications
With which buffer memory should the QoS, Retain, Will and Clean Session functions of the MQTT communication function be configured?
Answer
The QoS, Retain, Will, and Clean Session functions of the MQTT communication function can not be configured in buffer memory.
Module FB: M+FX5ENET. QoS can also be set with M+FX5ENET MQTT PublishSend(MQTT data transmission) and M+FX5ENET_MQTT_Subscribe(Subscribe command transmission).
- Product Name
- FX5-ENET
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series