FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding cable diversion to FX5-2HC/ES
FAQ
Regarding cable diversion to FX5-2HC/ES
Is it possible to use the connector cable when replacing the FX3U-2HC with the FX5-2HC/ES?
Answer
The cable cannot be used because the connector shape is different, so change the wiring.
FX5-2HC/ES is a spring clamp terminal block, and FX3U-2HC is a MIL-C-83503 compliant connector.
FX5-2HC/ES is a spring clamp terminal block, and FX3U-2HC is a MIL-C-83503 compliant connector.
- Product Name
- FX5-2HC/ES
- Product Category
- High-speed counter
- Series
- MELSEC iQ-F Series