FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the differences between the FX5-2HC/ES and the conventional FX3U-2HC input formats
FAQ
Regarding the differences between the FX5-2HC/ES and the conventional FX3U-2HC input formats
Is there any difference in input format between FX5-2HC/ES and FX3U-2HC?
Answer
The FX5-2HC/ES supports differential line drivers (5 V) only.
The FX3U-2HC supports open collectors (24 V/12 V/5 V) and differential line drivers (5 V).
The FX3U-2HC supports open collectors (24 V/12 V/5 V) and differential line drivers (5 V).
If you are using an open collector (24 V), consider replacing it with an FX5 CPU Module built-in high-speed counter or a high-speed pulse input/output Module.
- Product Name
- FX5-2HC/ES
- Product Category
- High-speed counter
- Series
- MELSEC iQ-F Series