FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding FX5-2HC/ES restrictions
FAQ
Regarding FX5-2HC/ES restrictions
Are there any restrictions on the FX5-2HC/ES system configuration?
Answer
The FX5-2HC/ES must be connected to the eighth module from the power supply module (CPU Module, expansion power supply module, built-in power supply I/O Module).
If the FX5-2HC/ES is added to the 9th or later module from the power supply module in GX Works3, a warning is displayed. The model selection tool does not allow you to select after the ninth model.
If the FX5-2HC/ES is added to the 9th or later module from the power supply module in GX Works3, a warning is displayed. The model selection tool does not allow you to select after the ninth model.
- Product Name
- FX5-2HC/ES
- Product Category
- High-speed counter
- Series
- MELSEC iQ-F Series