FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding Input Response Frequency Difference between FX5-2HC/ES and Conventional Model (FX3U-2HC)
FAQ
Regarding Input Response Frequency Difference between FX5-2HC/ES and Conventional Model (FX3U-2HC)
Is there a difference in input response frequency between FX5-2HC/ES and FX3U-2HC?
Answer
The input response frequencies of the FX5-2HC/ES and FX3U-2HC differ as shown below.
FX5-2HC/ES・・・2MHz
FX3U-2HC・・・200kHz
FX5-2HC/ES・・・2MHz
FX3U-2HC・・・200kHz
- Product Name
- FX5-2HC/ES
- Product Category
- High-speed counter
- Series
- MELSEC iQ-F Series