FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding connecting to AWS IoT Core Using the TCP Protocol
FAQ
Regarding connecting to AWS IoT Core Using the TCP Protocol
Is it possible to connect to AWS IoT Core using the TCP protocol with the MQTT communication function of FX5-ENET?
Answer
Because the AWS IoT Core specification is the TLS protocol, you cannot connect using the TCP protocol.
- Product Name
- FX5-ENET
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series