FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding using the connector of the CPU Module
FAQ
Regarding using the connector of the CPU Module
Can I use the I/O connector when replacing the FX3GC/FX3UC basic module with the FX5UC CPU Module?
Answer
The input/output cables used in the FX3GC and FX3UC basic units can be diverted to the FX5UC CPU Module (connector type).
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module
- Series
- MELSEC iQ-F Series