FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding using the MQTT Communication function in a local environment
FAQ
Regarding using the MQTT Communication function in a local environment
Is it possible to perform MQTT communication functions in a local environment without using the cloud?
Answer
Yes, you can use MQTT communication function even in the local network by preparing a personal computer with MQTT broker such as Eclipse Mosquitto installed.
*Eclipse Mosquitto is a registered trademark of Eclipse Foundation.
- Product Name
- FX5-ENET
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series