FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding sending files in an SD Memory Card by Mail
FAQ
Regarding sending files in an SD Memory Card by Mail
Is it possible to send SD memory card files (such as logging data) using the e-mail function?
Answer
Yes, as long as the capacity is expandable to the file register (R), it can be transmitted by using the file operation instruction.
When sending, please set the attachment format to BIN format.
When sending, please set the attachment format to BIN format.
- Product Name
- FX5-ENET
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series