FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding CC-Link IE field CPU module status during communication error occurs on CC-Link IE Field Network Basic
FAQ
Regarding CC-Link IE field CPU module status during communication error occurs on CC-Link IE Field Network Basic
When the CC-Link IE Field Network Basic is disconnected, will the CPU module stop?
Answer
CC-Link IE field When a network such as Network Basic is interrupted, the CPU module does not stop and continues to run.
When the CC-Link IE Field Network is disconnected,
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- Network/Communication
- Series
- MELSEC iQ-F Series