Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 44612
  • Release Date : 2024/11/28 16:12
  • Print

Regarding number of occupied I/O points of intelligent function module

What is the occupied I/O point of the intelligent function module?

Category : 

Answer

The number of occupied input/output points per module is 8.  (Excluding some models)
Occupied I/O points: Since actual occupied I/O points cannot be assigned to 8 points, add I/O devices within the remaining number of points subtracted from the maximum number of points. The actual number of occupied I/O points cannot be allocated to 8 points.

Example:When adding 2 intelligent function modules to the FX5U-32MR/ES, the number of I/O points can be increased upto 336 points, which is obtained by subtracting 16 occupied points (for 2 intelligent function modules) and 32 I/O points of the CPU module from the maximum number of I/O points of the FX5U CPU module: 384 points.

*Number of I/O  points: 384 points are supported with firmware version 1.100 or later.

Product Name
FX5U, FX5UC, FX5UJ
Product Category
CPU Module
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries