FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding number of CH of CPU Module built-in Heating/Cooling PID control
FAQ
Regarding number of CH of CPU Module built-in Heating/Cooling PID control
How many channels can the built-in Heating/Cooling PID control function of the CPU Module support?
Answer
The CPU Module's built-in Heating/Cooling PID control function supports up to 16 channels.
The following firmware versions are required in order to use it.
FX5U/FX5UC: 1.320 or later
FX5UJ: 1.080 or later
FX5S: 1.040 or later
GX Works3 1.110Q and later
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module,Analog
- Series
- MELSEC iQ-F Series