FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding number of CC-Link IE field network Basic connections
FAQ
Regarding number of CC-Link IE field network Basic connections
What is the maximum number of connections per network in CC-Link IE field network Basic?
Answer
When the FX5 CPU Module is used as the master station, the maximum number of devices connected to 1 network is 16.
The following firmware versions are required to connect 16 devices.
FX5U/FX5UC: 1.110 or later
FX5UJ: 1.080 or later
FX5S: 1.040 or later
GX Works3 1.110Q and later
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series