Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 44653
  • Release Date : 2025/03/18 10:23
  • Print

Regarding Control response parameter of built-in PID Control of CPU Module

What is the difference between "normal" and "fast" control response parameter of built-in PID control of CPU Module?

Category : 

Answer

The control response parameter can set the response to the target value (SV) of PID control as either "normal" or "fast". The difference is as follows.
(1)When "Normal" is set, the time to reach the target value (SV) will be longer, but overshoot/undershoot will be suppressed.
(2)When set to "Fast", the time to reach the target value (SV) will be shorter, but the overshoot/undershoot will be larger.

For details, refer to the following manual.
MELSEC iQ-F FX5 User's Manual (Application)

Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module,Analog
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries