FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding CC-Link IE field network support of FX5 CPU module built-in Ethernet
FAQ
Regarding CC-Link IE field network support of FX5 CPU module built-in Ethernet
Does the FX5 CPU module built-in Ethernet support the CC-Link IE field network?
Answer
The built-in Ethernet on the FX5 CPU module does not support CC-Link IE field networks.
If you use a CC-Link IE field network, add an FX5-CCLIEF.
*The FX5-CCLIEF does not support the master function. Supports intelligent device stations.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series