FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software > USB driver for GT Designer3
FAQ
USB driver for GT Designer3
How can I check that the USB driver for GT Designer3 is installed on the personal computer?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software > HMI/GOT Screen Design Software
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
The following shows how to check that the USB driver for GT Designer3 is installed on the personal computer.
1. Connect the personal computer and GOT using a USB cable then turn on the GOT.
Or, connect the personal computer and the GOT using a USB cable while the GOT is on.
2. Press [Win] + [R] to display the [Run] dialog then enter "devmgmt.msc" to display the device manager.
3. Under "Universal Serial Bus controllers" in the list, check that "MITSUBISHI GOT2000 USB Controller" or "MITSUBISHI GOT3000 USB Controller" is displayed.
Figure 1

If "MITSUBISHI GOT2000 USB Controller" or "MITSUBISHI GOT3000 USB Controller" is not displayed or "!" is displayed next to the device, restart the personal computer or reinstall the screen design software.
* The folder paths for the USB drivers are as follows:
(When screen design software is installed with the default settings)
• 32-bit OS
C:\Program Files\EZSocket\EZSocketGOT\Drivers\
C:\Program Files\MELSOFT\EZSocket\EZSocketGOT\Drivers\
• 64-bit OS
C:\Program Files (x86)\EZSocket\EZSocketGOT\Drivers\
C:\Program Files (x86)\MELSOFT\EZSocket\EZSocketGOT\Drivers\
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GT Designer3
- Series
- GOT2000 Series, GOT Screen Design Software, GOT3000 Series