FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > Engineering Software > Details of GT Works3
FAQ
Details of GT Works3
What type of product is GT Works3?
Answer
GT Works3 is screen design software for the GOT3000, GOT2000, and GOT1000 series, integrating functions inspired by a user-oriented perspective under the three themes of simplicity, tidiness, and ease of use.
GT Works3 includes the following software products.
• GT Designer3, GT Simulator3
• GT SoftGOT3000
• Data Transfer Tool
etc.
* GT Simulator3 is installed when GT Designer3 is installed.
For details on the GT Works3 lineup and licenses, refer to the following.
[FAQ][GT Works3 product configuration]
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GT Works3
- Series
- GOT Screen Design Software