Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 45308
  • Release Date : 2025/10/23 10:53
  • Print

Screen gesture function when the digital image input screen is displayed

Can the digital image input screen size be enlarged or reduced using the screen gesture function?

Category : 

Answer

The screen size cannot be enlarged or reduced because the digital image input screen is hidden during screen gesture mode.

* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture), GOT function (video/RGB)
Series
GOT3000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries