Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 45479
  • Release Date : 2025/11/12 13:54
  • Print

Regarding replacing FLT Instructions

An FLT command is input to convert an integer (16 bit) to a floating point on the iQ-F series, but the command cannot be determined.

Category : 

Answer

For the iQ-F series, use the following instructions.
For signed 16 bit integers, use the INT2FLT instruction.
For unsigned 16 bit integers, use the UINT2FLT instruction.

Product Name
FX5U,FX5UC,FX5UJ,FX5S
Product Category
CPU Module
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries