- No : 20778
- Release Date : 2018/08/21 16:10
- 
          
              Print
          
        
 
Differences between flange and face mounting 
    
      Please explain the difference between flange and face mounting patterns.
    
  
    - Category : 
- 
      
    
 
    Answer
  
    SHY right angle shaft type has lineup of flange and face mounting. For face mount type, screw hole processing is done on the flange surface of the gear case, and flange type is counterbored hole processing is done.
Please select according to the installation method of the equipment.
  
    
      
        - Product Name
- Geared Motors
        - Series
- Geared Motors Right angle shaft type, S-PM Geared Motors Right angle shaft type