- No : 20993
 
      - Release Date : 2018/08/22 16:25
 
        - 
          
              Print
          
        
 
  
 
Overseas inverter models
    
      What is the naming convention for the overseas inverter models? 
Are there any rules for kw?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    "□□□□□" in the model name of the FR-A700 series and FR-F700 series with the multiple ratings is as follows. 
"□□□□□" in the model name of the FR-A700 series and FR-F700 series with the multiple ratings is as follows.
FR-[A/F]7[2/4]0-□□□□□-NA/EC
- For the FR-A700 series in Europe (EC): SLD rated output current value
- For the FR-A700 series in North America (NA): ND rated output current value
- For the FR-F700 series in Europe (EC): SLD rated output current value
- For the FR-F700 series in North America (NA): SLD rated output current value
For example, when the rated output current value is 4.6 A, "□□□□□" is "00046", and when the rated output current value is 475 A, it is "04750".
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Product Category
 
          - Inverter
 
      
      
        - Series
 
          - FR-A700, FR-F700