• No : 20993
  • Release Date : 2018/08/22 16:25
  • Print

Overseas inverter models

What is the naming convention for the overseas inverter models?
Are there any rules for kw?
Category : 

Answer

"□□□□□" in the model name of the FR-A700 series and FR-F700 series with the multiple ratings is as follows.
"□□□□□" in the model name of the FR-A700 series and FR-F700 series with the multiple ratings is as follows.
FR-[A/F]7[2/4]0-□□□□□-NA/EC
- For the FR-A700 series in Europe (EC): SLD rated output current value
- For the FR-A700 series in North America (NA): ND rated output current value
- For the FR-F700 series in Europe (EC): SLD rated output current value
- For the FR-F700 series in North America (NA): SLD rated output current value
For example, when the rated output current value is 4.6 A, "□□□□□" is "00046", and when the rated output current value is 475 A, it is "04750".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-F700