- No : 21120
- Release Date : 2018/08/22 16:26
-
Print
FR-A700
For the A720-0.4K and 0.75K, the EMC filter is always valid." Why is the leakage current 1 mA?
- Category :
-
Answer
The leakage current is 1 mA because the circuit constant in the EMC filter of A720-0.4K and 0.75K are different.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700