• No : 21179
  • Release Date : 2018/08/22 16:26
  • Print

400 V inverter

Does the 400 V inverter run with 400 V input to the main power supply and 200 V input to the control circuit power supply?
Category : 

Answer

No, it does not run. "Err" is displayed when it is operated. Always input the same voltage (400 V) to the main power supply and control power supply.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-F700P, FR-F700