• No : 21187
  • Release Date : 2018/08/22 16:26
  • Print

Electronic bypass function

When using the automatic bypass sequence of the electronic bypass sequence, do I have to turn ON the MRS and CS?
Category : 

Answer

The signals MRS and CS are required when the automatic bypass sequence enabled.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-F700P, FR-F700