• No : 21189
  • Release Date : 2018/08/22 16:26
  • Print

Electronic bypass function

There are two patterns of the automatic bypass sequence in the electronic bypass operation sequence. What is the proper use?
Category : 

Answer

With the automatic bypass sequence (Pr.139 ≠ 9999, Pr.159 = 9999), the motor operation is switched to commercial power supply operation when the output frequency reaches Pr.139 and the inverter is used only for the acceleration/deceleration operation. With the automatic bypass sequence (Pr.139 ≠ 9999, Pr.159 = 9999), the motor operation is switched to commercial power supply operation when the output frequency reaches Pr.139. When the frequency command becomes less than the difference between Pr.139 and Pr.159, it is automatically switched to inverter-driven operation at the frequency by the frequency command. Therefore, use the commercial power supply for high-speed operation, and inverter for low-speed operation.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-F700P, FR-F700