• No : 21190
  • Release Date : 2018/08/22 16:26
  • Print

Electronic bypass function

When Pr.138 (Bypass selection at a fault) is set to "1", how can the commercial power supply operation be switched to the inverter-driven operation again?
Category : 

Answer

Turn ON and OFF the RES signal to enable the inverter-driven operation.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-F700P, FR-F700