• No : 21191
  • Release Date : 2018/08/22 16:26
  • Print

Electronic bypass function

Can I manually switch the operation to the commercial power supply operation at an inverter fault?
Category : 

Answer

The operation cannot be manually switched to the commercial power supply operation at an inverter fault. The operation can be automatically switched to the commercial power supply operation at an inverter fault. By setting Pr.138 (Bypass selection at a fault) to "1", the operation is switched to the commercial power supply operation at an inverter fault while the inverter running. Automatic switching is not available for the E.CPU.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-F700P, FR-F700