• No : 21192
  • Release Date : 2018/08/22 16:26
  • Print

Electronic bypass function

Is the electronic bypass sequence function available in the NET operation mode?
Category : 

Answer

No, it is not available. It is only available in the External operation mode or combined operation mode (PU speed command and External operation command (Pr.77 = 3).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-F700P, FR-F700