• No : 21193
  • Release Date : 2018/08/22 16:26
  • Print

Electronic bypass function

When the electronic bypass function is used, can the MRS signal (operation enable/disable selection) be normally closed contact by changing Pr.17 (MRS input selection) to "2"?
Category : 

Answer

No, it cannot be normally closed contact. When the electronic bypass function is used, the setting of Pr.17 is disabled.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-F700P, FR-F700