• No : 21245
  • Release Date : 2018/08/22 16:26
  • Print

Changing the control method

I want to change the control method to Mitsubishi standard gear motor GM-D for the operation. Which parameters should I set when changing the control method?
Category : 

Answer

Set Pr.71 (Applied motor), Pr.80 (Motor capacity), Pr.81 (Number of motor poles), and Pr.800 (Control method selection).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700