• No : 21252
  • Release Date : 2018/08/22 16:26
  • Print

DC reactor

In the list of options on the catalog of the FR-A700 (F700P), DC reactors (FR-HEL) are described up to 55K. Is the 75K or higher DC reactor available?
Category : 

Answer

The 75K or higher DC reactor is included in the 75K or higher inverter. The option cannot be purchased separately.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-F700P, FR-F700